This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I was facing the issue of the opamps heating when i just connect the power to it.I tried to test the functionality using it in non inverting mode and it did not show results.
Also tried this with mutliple ics, the heating persists, cannot figure out what the issue is.
Is there any other way to test the functionality.
I am providing around 5.7 volts as power.(+-2.85 volts to each power pin)
Any help would be appreciated
Hello Adit, welcome to the TI e2e forums.
Do you have the polarity correct and applying to correct pins? LMP7211 has an unusual pinout. Be sure to protect devices from ESD damage.
Try starting with a lower voltage and limit current to 10mA ; if you can't set current limit, add 100 ohms in series with VCC and VEE.