Other Parts Discussed in Thread: TLV7041, TL331B, TLV1861
Tool/software:
Hello,
I want to use this comparator (TLV7021/TLV7041) to monitor the input voltage of a device.
However, as the input voltage of the device can be as much as 36V, the supply voltage of the comparator is generated with an LDO that is located after some DCIN ramp up circuitry.
That means, that for some time the comparator is unpowered, but already has voltage at the input.
Another case is reverse input voltage. In this case, the comparator is unpowered (protection circuit prohibits neg. comparator supply), but there is a negative voltage at the input present.
My approach is to limit the comparator input current via appropriately dimensioned input dividers to <<10mA.
My questions:
- Is this sufficient/ok for long time reliability?
- The IC has internal ESD clamping diodes. At which voltage these diodes begin to conduct?
- Should I use additional external clamping diodes at the inputs to Vcc and Vee? If yes, do I need schottky diodes (see question 2)?
Many thanks in advance.