The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA253: The contradiction of INA253A1 between the theoretical and practical value

Part Number: INA253
Other Parts Discussed in Thread: TINA-TI

Tool/software:

Hi,

Theory Part

I have tried to run a test by using the software called LTspice. Below is the construction of my circuit. As observed below, the model "U1" that I use is INA253A1. This "U1" is downloaded from Texas Instruments page under the part of design & development.

After I click "Run" in my simulation, the diagram below is the result.

The desire outcome that I want to get for my "Vout" is 1 V when 10 A is supplied on the "I1", while "Vout" is -1 V when -10 A is supplied on the "I1". To achieve that, I have added in network resistors as shown on the diagram below.

After I click "Run" in my simulation, the diagram below is the result. This is the outcome that I want.

Until this part, above explanation concluded for the Theory Part.

Practical Part

I tried to build exactly the same setup based on my simulation on my practical PCB setup. However, the results that I have obtained are different with the "Theory Part".

I can get Vout = 1 V when I supply 10 A, while I can get Vout = -1 V when I supply -10 A without adding in the network resistors. This scenario shows a contradiction between the Theoretical value as well as the Practical Value. Can I know why I will get these reading with explanation. I look forward for the reply.

Thank you.

Regards,

Willie