Part Number: OPA855
Tool/software:
I am simulating the OPA855 to be used as a TIA. I am using LTSpice as that is the software I'm most familiar with. Attached below is the schematic, the circuit on the right is where I try to use the OPA855

You will notice two lib directives. Firstly I try to use the OPA855 spice model as is, in the same directory as the simulation file.
Unfortunately it complains about a pin mismatch.
....net(11): Number of nodes does not match number of pins (6) of sub-circuit "opa855".
X§U2 Ref N001 VCC VEE Vout_OPA855_A level1 OPA855 Avol=6.3k GBW=8000Meg Vos=0 En=0 Enk=0 In=0 Ink=0 Rin=500Meg
I worked around it by creating a copy of the OPA855 spice model and adding a dummy pin as such

And then specifying the sim file to use that file instead.
The simulation will now run however the results are bogus, for example the transfer function is as shown

The circuit should have 63.5 dB gain with a 3 dB cutoff at 100 MHz
Any help in correcting the simulation would be greatly appreciated.
Thanks,
Sojhal