This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM124AQML-SP: short circuit current and duration

Part Number: LM124AQML-SP


Tool/software:

Hello,

What is its short circuit current and duration? Within its datasheet, it lists its rated short circuit duration as continuous and the rated max as 60mA.

 

My question is what the actual max tested short circuit current is and the duration for which this was tested, if available.

Thanks, 

Adam

  • Hi Adam,

    What is its short circuit current and duration? Within its datasheet, it lists its rated short circuit duration as continuous and the rated max as 60mA.

    The table below is identified the short-circuit test conditions and it applies only to a single op amp per package when a short circuit is occurred. 

    what the actual max tested short circuit current is and the duration for which this was tested,

    LM124AQML-SP: The max. short circuit current is approx. -60mA to -70mA, depending on the Vcc and/or Vee. When the op amp's output terminal is shorted to GND, the current is sinking from the equivalent block diagram, thus the rating is shown negative. 

    If you have other questions, please let me know. 

    Best,

    Raymond

    HVA Application Team