Part Number: OPA855
Other Parts Discussed in Thread: OPA856, TINA-TI
Tool/software:
Hello,
I am currently designing a differential transimpedance amplifier (TIA) using the OPA855. My design is based on the paper "Wide-Bandwidth Low-Noise Simple Differential Transimpedance Amplifier Ideal for Detecting High-Frequency Faint Optical Signals" by Zhiyuan Wu, Zeyang Wen, Wenqiang Li, and Gongliu Yang.
However, I am facing an issue where oscillation occurs at the output. I used the feedback capacitor calculator provided by TI as a reference, but no matter how I adjust the capacitor value, the oscillation (around 500 MHz) persists. The only change observed is in the frequency range where peaking occurs in the output FFT.
When I simulated the same circuit in TINA, it was stable, as shown in the attached image.

and the image below shows the FFT of the output when only the supply is applied to the current board. It confirms that oscillation exists in the hundreds of MHz range.

To identify the root cause, I looked into TI’s forum and came across a response from kai klaas69 mentioning that the gain stability condition (7V/V) of the OPA855 was violated in a similar case. The link to the post is as follows:
TI forum link: e2e.ti.com/.../opa855dsgevm-high-gain-peaking-on-evm
In my current TIA board, the two input terminals are separated by approximately 8mm, but this gap is not purely copper traces. It also includes a DC block capacitor (0805 size) for APD bias isolation, as well as the feedback resistor and capacitor(0402 size).
To ensure the noise gain stability condition (>7V/V) is met, I intentionally added C_cm between both input terminals and tested values ranging from 1pF to 5pF in 1pF increments. However, the oscillation remained unchanged.
I intentionally increased C_cm, which is included in C_TOT, to ensure that the noise gain exceeds 7V/V.
Additionally, I tried reducing the OPA855-APD path length by physically moving the APD closer, but the results were the same (this was only for testing, not intended for actual use). This led me to believe that violating the noise gain stability condition may not be the root cause of the oscillation.
Interestingly, when I replaced the OPA855 with the OPA856, which has a lower GBWP but is stable at 1V/V, the oscillation disappeared. I believe this was simply due to the reduction in bandwidth.
So far, I have attempted:
- Adjusting the feedback capacitor
- Ensuring the noise gain stability condition is met
Despite these efforts, the oscillation persists, and I am unsure of what to try next. I would greatly appreciate any insights or advice from experienced engineers.
Best regards,
Moon