This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903B-Q1: Implement a comparator circuit with 10V as a threshold

Part Number: LM2903B-Q1


Tool/software:

Hello, Team,

Our customer is looking for a comparator which can input 10V as a reference and output 0V ~ 5V depending on the input signal (which would be 8~12V). Something like if above 10V, output = 5V and if below 10V, output = 0V. They are looking for a 2ch device so we think LM2903B-Q1 would be a best fit.

  1. Would LM2903B-Q1 meet the requirement?
  2. Do you have any other recommendations?

Best,
Masaru