This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA2290: Maximum leakage current into the IN+/IN- channels

Part Number: INA2290


Tool/software:

I will be using the INA2290 to measure current going into two other ICs on a power sensitive application. Regarding the Input Bias Current, are these combined leakage currents for each IN+, IN-? So for using the two channel device, even if the device is powered off, the combined total leakage current can be a maximum of (30uA + 30uA + 30uA + 30uA) = 120uA? That would be 30uA into each IN+1, IN-1, IN+2, IN-2.