Other Parts Discussed in Thread: AMC1200, AMC1351, AMC3330, ISO224
Tool/software:
Hello All,
I'm looking for a drop in replacement for the AMC1200-Q1 IC. Currently, this IC is being used to isolate two ground planes, it also receives and outputs differential signals. The main issue with our design is that we have to step down the source signal (+-5V) by a large (inverse) gain due to the AMC1200 input being +-250mV. As a result this node has high sensitivity. Just a couple of mV changes at the input of the AMC can have a large effect on the output stage of our design. So, we are now looking for a replacement (of the AMC1200) that has higher input voltage range, may be 1V peak to peak or higher. Our design is for DC application only.
Thanks.