Other Parts Discussed in Thread: OPA856, LMH34400
Tool/software:
I want to use the LMH32401 as a transimpedance amplifier with analog bandwidth of at least 250MHz. I prefer to have single ended output at 50 Ohms load. What is the most proper ciruitry I should use at the Out+ and Out- in order to get single output at 50 Ohms. What is the maximum output voltage level I can get at 50 Ohms ? I am going to implement the whole circuit on FR4 20mils thick material. Should I take special care on the bottom layer ground ? (e.g have ground voids beneath certain components in order to reduce parasitic capacitances. It would be also nice to provide me a TINA circuit model to test myself the behaviour of the proposed circuit.
Thanks,
Yorgos