This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA181: INA181

Part Number: INA181


Tool/software:

Hello TI team, 

I am planning to use the Current sensing Opamp INA181A1 and INA181A2 with one of my recent project. I had a query if I will use this to sense a current which is specified as below:

1. Max DC current 12A

2. AC ripple frequency is 100 kHz

3. Sense resistor is 6 mOhm.

Here, I had a query if this Opamp is suitable to measure the Shunt voltage at this frequency???

Rshunt is placed at output of the buck converter, after LC filter.

Thanks 

Chetan Shishangiya