This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA172: Current shifter for VCc=5V instead of VCc= 12v

Part Number: OPA172
Other Parts Discussed in Thread: OPA2197, OPA197

Tool/software:

Hi sir ,


last Year we have communicated for Current level shifter circuit .

we have used P1 = XP9561GI

N1 = 2N7002 FOR following circuit which bias by VCc= +12V , but now we required biasing for VCc=+5V .

can it be possible with same P1 and N1 .

Today I have reduced VCC From 12v to 8 V then also load current required are stable but for below 8V load current reduced . 

I had attached simulation circuit provided by Mr. Ron mac... Sir