Other Parts Discussed in Thread: LM2904B, , ALM2402-Q1, ALM2402F-Q1, ALM2403-Q1
Tool/software:
Hi all,
I've been looking for an opamp to use as a VCOM buffer.
Supply Voltage range:~ +7V/-7V
Output voltage range: -3V to 3V
Stable with capacitive load (~10uF)
Output current ~50mA
AEC-Q100 grade 2
I think the LM2904B matches this, but I'm unsure of the stability.
Can anyone comment on that?
Thanks.
KR