Part Number: INA237
Tool/software:
Hi,
I have a question about the I²C timing requirements for the INA237, as specified in section 6.6 “Timing Requirements (I2C)” of the datasheet. The parameter t_HDDAT(Data hold time) is given as Min = 10 ns and Max = 900 ns. I’m not sure which of the following two interpretations is correct:
1.Slave-to-Master transfer: When the master reads from the INA237, the INA237 will update SDA at some point between 10 ns and 900 ns after the falling edge of SCL. Therefore, the master must sample the data before the slave’s update window.
2.Master-to-Slave transfer: When the master writes to the INA237, the master must drive SDA between 10 ns and 900 ns after the falling edge of SCL.
Which interpretation is correct? Any clarification would be greatly appreciated.
Thank you!