Tool/software:
I am looking through the Datasheet and found a section near the absolute max section saying "Input terminals are diode-clamped to the power supply rails. Input signals that can swing more than 0.5V beyond the supply rails should be current-limited to 10mA or less." Does this apply to situation where input signals may be continuously run beyond the voltage rails? For example, if the voltage rails were +5.0V and 0.0V, could the input signals be run continuously at -0.7V or 6.0V as long as the current is clamps to 10mA or less. How does this effect the lifetime of the part?