Part Number: INA191
Other Parts Discussed in Thread: INA199, INA2191, INA241A
Tool/software:
Hello,
In existing design we are using AZ-0500 1:500 (Talema) current transformer and TLV9002ID* to measure 400VAC 50/60Hz
Primary current range: 62.5mA(min) and 9A (max in failure state) which reflects to min secondary current of 125uA and maximum of 20mA (burden resistor is 30 ohms)
To increase the accuracy i was thinking to use INA199 as per the note TIDA 00753.
The issue i see is the high biasing current of 28uA, comparable to secondary current mentioned above(125uA).
We have 2 channels, so INA2191 looks closer to the our requirements considering dual channel and low input bias current. We will connect Ref pin to 2.5V.
Query: 1 The figure 7.2 INA2191 Diagram shows capacitive input in series which is slightly confusing how it process DC input?
Query: 2 Do you think, we can go with INA2191 for AC current sensing or some other better solution.