Other Parts Discussed in Thread: LM2903B, LM393LV
Tool/software:
Hi Team,
I have a design which uses the LM2903B comparator. It runs on Vcc=4.2V. One of the inputs is fixed at 2.3V, while the other varies between 0.3V and 3.9V.
The datasheet states the VCM at ambient is Vcc-1.5 ( = 2.7V) so everything should work fine (at least one input is within VCM).
However, across temperature the VCM reduces to Vcc-2 ( = 2.2V), so the comparator may not work in this situation.
App Note SNOAA5F (https://www.ti.com/lit/an/snoaa35f/snoaa35f.pdf?ts=1748330538078) page 17 seems to suggest the VCM gets worse as temperature decreases.
"The input range from 0 to 3.5V (VCC - 1.5V) is valid at 25°C and above." ... "This results in the input voltage range changing at -4.2mV/°C over temperature (note the negative sign!), necessitating the VCC - 2V over temperature specification."
Am I understanding this correctly? At temperatures between +25C and +125C, I can assume the VCM is Vcc-1.5? And temperatures below +25C, I can derate the VCM at -4.2mV/C? My device needs to operate up to 95C so, if true, this would solve my issue.
As a side note, if I derate at -4.2mV/C from +25C down to -40C, the VCM should reduce by 65*4.2 = 273mV. This should mean the VCM across temperature is Vcc-1.773, not Vcc-2. Is the extra allowance just safety margin, or is there some additional factor that I'm missing.
Best Regards,
Chris