This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4310: ESD

Part Number: OPA4310
Other Parts Discussed in Thread: OPA4348, OPA2348, OPA348

Tool/software:

Hi team,

we know that OPA4310's Input pins can swing beyond (V+) as long as they stay with in 6.0 V, there has No diode structure from input pins to (V+). The datasheet says OPAx310 features no current-steering diodes connected between the input and positive power supply pin. are they snapback ESD? Or it's just steering diode for TI's amplifier products (I see some comparator products say there has snapback ESD)? thanks.

In addition, OPA4348 doesn't have diode structure from input pins to (V+) neither, while the datasheet spec shows the max Common-mode voltage at input is (V+) + 0.5V. if there has no diode-clamp to V+, why the max common-mode voltage at input is not a fixed value (such as 6V in OPA4310)?

thanks a  lot.

Best regards,

Yang