Tool/software:
Hello,
As per datasheet OPA4872-EP it is mentioned that operating supply voltage is +/-5V.
Is this device operating with unipolar voltage 0 to 5V?
Input at mux would be 0 to 3.3V.
Thanks,
Nilesh Karale
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
As per datasheet OPA4872-EP it is mentioned that operating supply voltage is +/-5V.
Is this device operating with unipolar voltage 0 to 5V?
Input at mux would be 0 to 3.3V.
Thanks,
Nilesh Karale
Hi Nilesh,
This device requires a minimum supply of 7V. I would add that this device along with other devices that are not rail to rail would not work with a single supply and an input of 0V as both input and output range of the device requires some headroom to either supply.
Best Regards,
Ignacio