This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4872-EP: Operating supply voltage

Part Number: OPA4872-EP


Tool/software:

Hello,

As per datasheet OPA4872-EP it is mentioned that operating supply voltage is +/-5V.

Is this device operating with unipolar voltage 0 to 5V?

Input at mux would be 0 to 3.3V.

Thanks,

Nilesh Karale 

  • Hi Nilesh,

    This device requires a minimum supply of 7V. I would add that this device along with other devices that are not rail to rail would not work with a single supply and an input of 0V as both input and output range of the device requires some headroom to either supply.

    Best Regards,

    Ignacio