Part Number: TLV1391
Other Parts Discussed in Thread: TL331B, TL331LV, TL331,
Tool/software:
Hi team,
Do you have recommendation of NJM2406F-TE2 alternative?
Thanks
Lillian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Lillian,
There is also the TL331LV and TL331B. Both are a bit slower.
Note that the TL331 pin-out has reversed inputs from the standard SW pinout - so be careful when crossing.
| ► Part Number | NJM2406F | TLV1391IDBVR | TL331BIDBVR | TL331LVDBVR |
| Manufacturer | NJR | TI | TI | TI |
| Pinout | TL331 Southeast with Rev Inputs | TL331 Southeast with Rev Inputs | TL331 Southeast with Rev Inputs | TL331 Southeast with Rev Inputs |
| Channel Count | 1 | 1 | 1 | 1 |
| Package | SOT-23-5 | SOT-23-5 | SOT-23-5 | SOT-23-5 |
| Package (TI Equiv) | DBV5 | DBV5 | DBV5 | DBV5 |
| Vs min (V) | 2.5 | 2 | 2 | 1.65 |
| Vs max (V) | 7 | 7 | 36 | 5.5 |
| Response Time, typ (µs) | 0.5 | 0.781 | 1 | 0.6 |
| Vos max 25°C (mV) | 7 | 5 | 2.5 | 2 |
| Input Range | To V- | To V- | To V- | R-R |
| Output Type | OC | OC | OC | OC |
| IQ (max) (mA) | 0.8 | 0.125 | 0.33 | 0.035 |
| IBias (typ) (nA) | 20 | 40 | 3.5 | 0.005 |
| Temperature Min | -40 | -40 | -40 | -40 |
| Temperature Max | 85 | 85 | 125 | 125 |
| Additional Features | Vout>V+ | Vout>V+ | POR, FailSafe, Vout>V+ | |
| Auto Qual | ||||
| GPN | NJM2406 | TLV1391 | TL331B | TL331LV |
| Datasheet | NJM2406 | TLV1391 | TL331B | TL331LV |