This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA226: Overvoltage Protection for INA226 – Design Inquiry

Part Number: INA226


Tool/software:

Dear Texas Instrument Team, 

I hope that you are doing well. 


After reviewing the INA226 datasheet, I noticed that the VBUS and IN+/IN− pins do not include built-in overvoltage protection. As a result, I have been running simulations in LTspice to design an external overvoltage protection circuit, particularly for the VBUS pin.

The solution I developed appears to work effectively; however, it introduces a voltage drop due to the use of a MOSFET in series with the power input. I’ve attached circuit simulation images below for your reference.







I would greatly appreciate your assistance with the following:
• Could you suggest a more suitable overvoltage protection circuit that does not impact the VBUS input voltage accuracy?
• Optionally, do you have any recommendations for protecting the current-sense inputs (IN+/IN−) to ensure that the differential voltage across the shunt resistor does not exceed the maximum 81.92 mV input limit of the INA226?


Thank you very much for your support. I look forward to hearing from you.


Best regards.