Part Number: AMC1200-Q1
Other Parts Discussed in Thread: AMC1200, UCC28711
Tool/software:
Hello:
Pl take a look at the attached sch : it has AMC1200 amp in a very std way of isolated current sensing.
In the application, voltage across the current sensing resistor R2 is not allowed to exceed 300mv differential and inrush at turn-on voltage across R2 is clamped to safe levels for AM1200.
The source of the current through R2 is a DC-DC converter using UCC28711- but this is not relevant to the issue at hand.
Here is the issue we find .
With converter return current causing R2 voltage to be 140mV
Yet at pin 2, we notice only 90mV. Leakage & input offset etc do not seem to be causing this huge drop.
Second issue is that differential output of AMC1200 is expected to be 8* 90 mV
But it is not. In fact output might be oscillating.
We have not yet taken clean waveforms.
While that effort is ongoing, we need to address this discrepancy.
-Why 90mV at pin 2?
-Why there is no gain at the outputs?
What needs to change for these numbers to be consisAMC1200_SCH_TI.pdftent with the Spec sheet expectations.
Any help will be highly appreciated
-r