This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9061-Q1: Output error at low voltage

Part Number: TLV9061-Q1
Other Parts Discussed in Thread: TLV9061, , AMC3302

Tool/software:

Hi Team,

I am using TLV9061-Q1 for converting differential to single ended output of AMC3302 for shunt based application. At lower voltage of shunt < 1-5 mV output of TLV9061 is not working as expected in simulation. I am getting 50mV as output in this case. When Input of TLV9061 is increasing  more than 50mV then its following input voltage as expected. Can you help me to solve this issue.

Regards

Vivek