This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA500: INA500B differential impedance tolerance and drift over temperature

Part Number: INA500

Hi,

Regarding INA500B, the datasheet specifies typical differential input impedance 2.88MOhm, and section 7.3.1 mentions -+15% tolerance of all of the resistors.

We are considering calibrating our analog errors at room temperature, therefore I would like to differentiate between the unit to unit error (in room temperature), and the temperature drift.

Can you supply more information regarding the differential input impedance tolerance? Either as min max or standard deviation.

Does the -+15% refer to minimum and maximum across temperature? Is it a tight tolerance?

Thank you

  • Hi Amit,

    This information is indirectly supplied through the gain error values. In fact, I think that would be more value to you all for compensating the gain. 

    Best Regards,

    Robert Clifton 

  • Hi Robert,

    In my design I have resistors in series with the amp input, so there is effectively a voltage divider between the input differential impedance of the amp and the mentioned external resistors. The voltage at the amp's input terminals depends on the input differential impedance.

    So, unrelated to the gain error of the amp, there is an error in the division ratio. The input diff impedance has high tolerance (-+15%), and the system is 12bit accuracy, so this error is not negligible.

    I am considering calibrating the analog errors at room temperature, therefore I would like to differentiate between the unit to unit error (in room temperature), and the temperature drift.

    Can you supply more information regarding the differential input impedance tolerance? Either as min max, or standard deviation.

    Does the -+15% refer to min and max across temperature, or in room temperature?

    Is there any data regarding temperature drift of the input differential impedance?

    Is -+15% a tight tolerance?

    Thank you,

    Amit.

  • Hi Amit,

    So, unrelated to the gain error of the amp, there is an error in the division ratio. The input diff impedance has high tolerance (-+15%), and the system is 12bit accuracy, so this error is not negligible.

    I'd like to clarify that the datasheet says that the resistor values can vary together up to +/-15%. One internal resistor will not shift +15% and another shift -15%. 

    I'll ask the design team about this. 

    In the meantime, how much resistance are you planning on adding to the input? 

    Best Regards,

    Robert Clifton 

  • Hi Robert,

    The series resistance is significant, compared to the 2.88Mega Ohm of the amp and the required accuracy. On the order of hundreds of kilo Ohm.

    I would like to emphasize that I don't care about each resistor in the amp, I care about the "total" differential input impedance,

    Specifically, room temperature tolerance and temperature drift, either as min\max or standard deviation.

    Thanks, Amit.

  • Hi Amit,

    I'm still waiting to hear back from the design team.

    When you are using hundreds of kilo ohms on the inputs, we typically recommend using an instrumentation amplifier instead to eliminate the distortion caused by any mismatch on the input resistors as well as general gain and CMRR degradation that will occur. 

    Is there any reason that you decided to use a difference amplifier rather than an instrumentation amplifier? 

    Best Regards,

    Robert Clifton 

  • Hi Amit,

    Sorry, I had forgotten that this is INA500B and not INA500A. 

    Design got back to me and informed me that you can expect the resistances to change less than 50ppm/C. The resistors are fairly linear across temperature. 

    Also ±15% is 3.5-sigma and ±22% is 5-sigma. 

    Best Regards,

    Robert Clifton