This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3470: DIE_TEMP output not working

Part Number: THS3470

I am using a Rev. B chip in a 10 MHz, +/-25V application. So far, it is working well. However, the DIE_TEMP output is not working.  With no load, the output is static at ~1.8V, no matter the temperature. VMID and VDD are stable at 0V and 5V, respectively.
Please help.