This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA592: Voltage to Current converter Using INA592

Part Number: INA592


INA592 is used for Voltage to Current conveter. My circuit expected to work as

i. Sink mode Configuration:  Vin below 1.25V current(0-20mA) should flow and if Vin  above 1.25V then 0mA should flow.

above is working fine if My INA592 Supply and Loop Resistor R7 connected to same supply.

But when INA592 Connected to 33V and Loop Resistor R7 connected to 24V with common ground. The circuit is working for Vin from 0-2.5V and current is varying from -20mA to 20mA.

I have attached the schematic and waveform. Scheatic.jpg

image.png