Part Number: TLV9052
Other Parts Discussed in Thread: PGA900, ADS1115, INA819
Sorry up front if this is in the wrong place in the forum. I need some help choosing a device & design I can use to interface a load cell to a BeagleBone Black Rev C. MCU. I couldn't post this without choosing a TI Part number and we use the TLV9052 already.
I have a VPG Force Sensors 60001-500L-A1-00F s-type load cell considered for a prototype weighing application on a new piece of stationary agricultural equipment. The load cell is a Wheatstone bridge type sensor. We plan to use four of these to measure the weight of the fluid in tank during or process.
I am an engineer but do not have much experience with load cells interfacing through milivolt outputs.
The load cell has a full span weight range of 0-500lbf. It's sensitivity is 3.000mv/V and the maximum excitation is 15VDC and 10VDC is the recommended excitation. It will be easiest for us to excite the load cell with 12VDC.
We use the BeagleBone Black Rev C microcontroller and my preference, not a hard or fast requirement, is to interface with I2C. The BeagleBone's I2C voltage range is 0 - 3.3V.
I have attempted to use the Nuvoton NUA7802 ADC on a breadboard to interface this and just can't get that to work. I think part of the problem is that the load cell needs an excitation voltage higher than the ADC likes. I haven't blown anything up but the readings are not right.
I am confident that TI has a good option but haven't been able to identify one. I know TI will have better documentation, tips and support! The TLV9052 is not my suggestion. I Just had to choose a part number to be able to post something here. The PGA900's are going to be hard for us to prototype with on a board unless you have suggestions of mounting methods I could use to handle it manually on a breadboard.
I look forward to hearing suggestions.
WC