This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA855-Q1: Power supply range for OPA855

Part Number: OPA855-Q1
Other Parts Discussed in Thread: OPA855

Hi

 

I saw the recommended power supply range is 3.3V~5.5V for OPA855 in datasheet, looks it is hard to use 3.3V to power OPA855, a little drop on power line will be over the spec, is the actual minimum supply voltage really 3.3V? 

 

Thanks

Bruce

  • Hi Bruce,

    Yes, the minimum supply of 3.3V is needed for proper operation of OPA855. Though the device may work for supplies slightly less than 3.3V but the performance and specification as per datasheet cannot be guaranteed at supplies <3.3V

    Regards

    Anant