Other Parts Discussed in Thread: TAS2781
Linux Kernel: 6.6
Tas driver Link: tas256xsw-android/tas2563-android-driver - Software for TAS256x on Android Platforms - TAS2563 Android Driver
Tas2563 Firmware: tas256xsw-android/tas2563-android-driver - Software for TAS256x on Android Platforms - TAS2563 Android Driver
Integration of the TAS2563 driver on Linux kernel 6.6 has been completed, and the snd-soc-tas2563.ko module is present. Added the firmware files on the IMX95 board and restarted, upon bring up, OS loads driver successfully, and the aplay command detects the sound card.
Log information is attached.
Issue: When attempting to play WAV files using the aplay command (as shown in the logs), there are no errors reported, but no sound is heard from the speaker.
Please let me know if any additional information is required to resolve this issue and bring the system to a working state.