Other Parts Discussed in Thread: TLV3511
I'm creating a circuit to detect diode conduction across a FET for synchronous rectificaiton. I've noticed some strange behaviour when simulating the TLV3511 in LT spice using the TI provided PSpice model. I wanted to confirm what the real behaviour of the device would be in this situation. I've attached a screenshot, I'll explain what's going on there:
- The voltage at Vds (pink) rises, causing the comparator output to go low initially as Vds goes above 0V (the set trip point).
- BSS123 starts to turn off but isn't quite fast enough, allowing the voltage at IN- to rise above 5V.
- During the time where the TLV3511 IN- input is above 5V (specifically above 5.2V), the output sits at a half rail value
Is the behaviour described in point 3 real? I would find it strange that activating the internal protection structure would cause the output state to change. Considering the comparator inputs would still be putting the output in a low state. It's also strange that the voltage is able to increase up to 5.7V, rather than being clamped at 5.3V. 
Thanks!
Aaron