Part Number: INA2180-Q1
Other Parts Discussed in Thread: INA2290, INA2180, INA2181
Hi team,
Customer plans to use INA2180-Q1 on EMB and wants to know how to design to pass 35V@400ms load dump test.
Customer is considering designing based on the following circuit according to the datasheet. Are there any recommended Zener diodes? Or what parameter requirements should they meet? Or does team have any recommended circuits?
If the above circuit is selected, customer has the following problems.
- If a 22V Zener diode is selected, there will be a voltage difference of 35V-22V=13V between the Zener diode and the power supply during load dump, resulting in a large power dissipation of the resistor. What value of resistor should be selected?
- The maximum common-mode input of the INA2180-Q1 is 28V. How is this value determined? Is it permissible to exceed this value?
- Are there any other multi-channel current-sense amplifiers with a common-mode voltage greater than 40V that you would recommend?
BR,
Jade Lan