This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA188: INA - Will Super-Balance topology improve offset drift?

Part Number: INA188
Other Parts Discussed in Thread: NE5532, OPA191, , INA592, THP210, ADS127L11

This could be an extension question to the following Forum Question.

"NE5532: Superbal circuit" - over 5 years ago.


Hi,

The circuit is part of a precision measuring instrument. Therefore I am interested in INA drift versus the (4) internal resistor(s) heat. 

Super-Balanced Diff Amp.png

Added to an Instrument Amplifier (INA188), is a Super-Balanced circuit (4 Opamp Instrumentation Amp). The 4th Opamp will be the OPA191.

With a 3 Opamp Instrument Amp circuit, there will be different power dissipated in each resistor string (R1+R2 versus R3+R4). In the 4 Opamp topology, the balancing makes the power dissipation in each string - the same.

Does the Super-Balancing improve/stabilise the offset drift due to "internal" resistor heating?

INA188 OPA191 AMP.TSC 

Will a precision circuit benefit from doing this? 

Thanks

Regards,

Peter Baxter

Might I be able to get an email address to send a simulation file - which is not public?

  • Hi Peter,

    Just to clarify, you are now using the INA188 in place of the more discrete implementation? 

    Best Regards,

    Robert Clifton

  • Hi Robert,

    I was originally using a MSOP8 4-Resistor package. Then moved to the INA592. Finally changed to the INA188. I'm going to use the OPA191 because of a recent forum question where Art Kay suggested that I use it (for another reason).

    Further to this, I have the FDA (THP210) ADC (ADS127L11). FDA's require a similar balanced 4 resistors. But around the resistors there needs to be an anti-alias filter. I ponder wouldn't it have been nice to have a precision resistor set inside FDAs. But its asking too much.

  • Hi Peter,

    Thanks for clarifying. I'll move this post over to the right team that can help you with this. 

    Best Regards,

    Robert Clifton 

  • Peter,

    Can you please restate and clarify your questions.  

    1. Draw the precise circuit you want to discuss with all the amplifiers, and components correctly identified.
    2. If temperature drift is a concern I need to know the specifications for any discrete resistors as well.  If it is a resistor network, let me know the model number.  If it is a discrete resistor, let me know the temperature drift (e.g. 25ppm/C).
    3. Restate your question and refer to your posted schematic in your question statement.

    Best regards, Art

  • My apologies here.

    I re-looked at the Super-Balance circuit and my concept of what was happening inside was not correct. 

    Hence the question is irrelevant.

    Thanks for responding.

    Regards,

    Peter Baxter