This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4898: Reg: LM4898MM (VSSOP-10) used to amplify single ended audio signal

Part Number: LM4898

Hi TI Team,

I have 16/32 ohm single-ended headphone output (up to 20mW) from Soc.

I need to drive an 8ohm/1Watt speaker, so that i have used LM4898MM(VSSOP-10) IC as a power amplifier.

In datasheet, application circuit is given for differential audio input circuit (Figure 4.), but i want to use this IC for Single ended audio signal. can you provide me the reference circuit design for single ended audio signal.

Thank you. Regards