I know this is long but please hang in there I need help on this please.
We are using the two op-amps in an OPA2171 as a window comparator.
This is the hardware setup.
VCC = 12VDC signal supply
MAX4080SASA current sensor amp with the output connected to the inputs of the OPA2171 on pins 3 and 6
Outputs of the OPA2171 pins 1 and 7 to a CD4001 setup as a Flip-Flop.
Two 20K ohm 25 turn trim pots connected to VCC and GRN with the wipers to inputs 2 and 5 of the OPA2171 to set references inputs.
What I'm seeing and don’t understand is as follows?
With the output of ~0V from the MAX on pins 3 & 6 of the OPA2171.
Pin 2 of the OPA2171 is set at 1.85 using one of the 20K trim pots.
Pin 5 of the OPA2171 is set at 1.65 using one of the 20K trim pots.
As the voltage on the input pins 3 & 6 from the current sensor increase the reference voltages on pins 2 & 5 also increase?
It is like there is current flow between the two input pins (it’s like a low resistances between the each pair of pins)?
I have checked the pins of the OPA2171 not installed and pin 2 to 3 is ~ 48K ohms.
I have removed the OPA2171 from the PCB and checked the PCB and found nothing.
I am able to set the trip point of each op-amp without issues and the circuit works in our application but I need to understand what it is doing and why.
I found this trying to setup a test and cal procedure for production.
So I went back to my prototype and found out that it was using the OPA251 not the OPA2171!
Someplace along the line it was decided to change from an OPA2251 to a OPA2171 because of cost.
Notwithstanding I check the prototype and it did not have this quirk.
It worked as you would think the references inputs stayed the same all the time no manner what the other inputs where doing.
If I was to use just the outputs to setup the unit I would not even know this was going on.
Thanks for all your patience and your comments.
Tom