Part Number: OPA855
Other Parts Discussed in Thread: OPA830, LMH6611
Hello, E2E
I'm jonghyn
I want to design howland current pump using TI product. so i download PSPICE for TI and simulate it.
My design target is maximum 0.75mA +- 0.75mA (1kHz - 100MHz) and driving load impedance, 10 ohm - 1.6kohm.
1. So as shown attached file below, when i use ideal OPAMP and use 1kohm, I can get proper calculated load current (0.5mA +- 0.223mA). but i change ideal OPAMP to OPA855 with VCC = 3.3V & VEE = 0V, DC current is move to 2.75 mA. what happen to it?
2. Can you recommand to me suitable OPAMP product for me?
(Maximum current target: 0.75mA +- 0.75mA (1kHz - 100MHz) and Load voltage is change to 550 ~ 800 mV)
3. If you recommand to use improved Howland current pump using additional buffer (, Hope to recommand proper buffer OPAMP.