Part Number: LMP2012QML-SP
The datasheet of the LMP2012QML-SP OPAMP specifies the absloute maximum limit of the supply voltage to be 5.8V. Do i understand correctly that this referes to the voltage difference between the two supply pin i.e. V+ - V-? So using this part with V+=+5V, V-=0V or V+=+2.5V, V-=-2.5V is ok but V+=+5V, V-=-5V would exceed the specification.