Hi TI Engineers,
On the datasheet of OPA657, page 11, it said that unity-gain stability in the op amp is not required for application as a transimpedance amplifier.But I was wandering why?
If the I-V circuit can be seen as a UNITY GAIN voltage amplifier, the unity-gian stability must be required!
OPA657 has a high gain bandwidth product 1.6GHz and very low noise performance, so can I use it in the following circuit if i got a high-ohm resistor with very low parasitic capacitor.

Thanks!
Eva
if the fc is large enough ,we will get small feedback capacitor,even though Cin is hundred pF or 10nF. That is why I choose 657. Of course, all above is on the condition that the 500Mohm resistor has a very small parasitic capacitor.