Hello everybody. I’m designing a system for acquiring a current signal using the logarithmic amplifier LOG112. I would like to use a 16-bit ADC like the ADS8505. However, I’m not very sure how to interconnect these two devices: is enough to connect the output of the LOG112 to the input (resistance network as shown on fig. 21 on pag. 10 of its datasheet)? Or should I use an operational amplifier (voltage follower) in between both of the for impedance couple? I’m using the LOG112 internal operational for scaling my current range to the desired output voltage (as shown on the figure on the first page of its datasheet). I haven’t found any information about this on the technical documentation.
Thank you very much for your help in advance.