My application is a low noise charge amp. Thus, knowing the CM and DM input capacitances is important for predicting the white input referred voltage noise density. Unfortunately, the datasheet for this device does not list values for these parameters. So, to see if the model included them, I ran simulations of the input capacitance measurement circuits shown in Figure 8.8 on page 97 of Bob Pease's book Troubleshooting Analog Circuits. The values I obtained were so improbably small that I concluded that they weren't part of the model either. Has anyone characterized them?