I'm running ORCAD v16.3.
I set the simulation up in accordance to the following recommendation from the model, itself:
* ADD .OPTIONS ITL=40 AND .OPTIONS GMIN=10p TO NET LIST IF SIMULATION DOES NOT
* CONVERGE
I get the following statements in the output file, after the smiulation aborts:
**** Capacitor MODEL PARAMETERS
******************************************************************************
X_U1.CP1P2
C 1
ERROR -- Convergence problem in bias point calculation
Last node voltages tried were:
I've experimented with ORCAD's Autoconverge options. But nothing seems to help.
Does anyone have any other suggestions?