Hello,
Does the REF3012 support a 1.71V input at output loads between 50-100uA?
I see conflicting notes in the datasheet that say:
Note 1, Minimum supply voltage for REF3012 is 1.8V, but then a little above that in the power supply section the min spec over temp is Vref + 50mV (min).
We are using the REF3012 on a number of our boards with a 1.8V supply that could dip as low as 1.71V (3% tolerance).
Thanks,
Steve Logan
Xilinx