I am using the TLV3401 comparator in a design where I currently have the open drain pull-up voltage set to +3.3V while powering the device with a single +5V supply. This is working properly as it is now but I would like to change the pull-up voltage to +1.8V. I could not find any pull-up voltage requirements on the datasheet for the comparator's output so I want to make sure that part will continue to work as intended with the +1.8V. Thanks for your time.