Hello,
I'm trying to make a voltage-controlled current source to control a laser module (Flexpoint dot laser module 635nm, 4mW, DC 4.5-30V).
I want to provide a limited current (0-100mA) according to its modulation voltage (0-5V). 0V is maximum current, 5V is minimum current.
The graph shows the I-Vmodulation measured curve overlapping the therotical I-Vmodulation curve provided with INA105 and OPA633.
The INA105 with OPA633 works very well. I set V2 as the modulation voltage, R as 107Ohm and V1 as 8.19V but when I connect the laser module I get a totaly different rail that is much lower (40 to 33mA).
I don't understand why the laser module somehow can change the current source.
Is there a way to 'isolate' the current source? Does this make sense?
I use TINA for simulation but I'm not sure there is a model for a laser module. If you know one or can offer an other equivalent model I'd be very interested.
Thanks
Charly