Dear Sir,
I wanted to use a filter amplifier circuit using op-amp which pass up to 30MHz frequency.
As this application is based on radar, there is going to be a lot EMI-EMC, could you please suggest some methods which will help in filtering EMI-EMC on the signal lines. I was going to common-mode chokes and pi-filters on the signal lines, will this be OK or do I have to add anything else?
I was intending to use OPA830. What op-amp do you suggest I use? The input range to the op-amp will 5Vp-p, I will bring it down to 2.5Vp-p with help of op-amp circuit itself. Also is this advisable?
Currently I am in the research stage of my project hence I am currently working on ideas and do not have any circuit to show as reference that I will be using.
Thanks Regards
Raquib Akolawala