Other Parts Discussed in Thread: OPA832
Hi all.
We are one company to control public lighting.
Now, we have designed one hardware product with OPA832 amplifier in order to have 1-10V control for ballasts. The ballast drives the lamp. With 0V, the lamp is off. With 10V, the lamp is in 100% power.
I write you because hardware product requires OPA832 amplifier in order to amplifier by 2 the input voltage, so it is no necessary to include the gain resistors regarding OPA832 datasheet.
The power supply is 10.94 volts.
We have made many units and almost all works well, but I saw one or two (of 50 pieces) that output of OPA832 is 0V. First, it worked good, but some days after, the output did not work, it is always with 0V.
Is any problem with OPA832 in single-supply mode powering with 10.94V (absolute maximum rating is 12V)?
I attach schematics.
Thanks in advance.
Francisco Jimenez.