Hello!
I'm assessing the possiblity of using a TL3474 quad OpAmp in order to replace an MC33074 (by ON Semi). I just need to confirm some information stated in datasheet. At last row of the table shown in page 4, it says that the Icc TYP is 3.5 mA per channel (for all cases). Then when I check the Figure 10 (in page 7), @25C says it is about 7mA. How do I match this information? Is the plot of Figure 5 for all the quad device?
Thanks for your help!