Hi!
Can INA226 measure pulse current / voltage? Interesting low side sensing. It need with pulse adjusted load. I load = 0...20 A, V load = 5...30 V.
What solution will be available in hardware or software (in triggered mode)?
Thank's!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
Can INA226 measure pulse current / voltage? Interesting low side sensing. It need with pulse adjusted load. I load = 0...20 A, V load = 5...30 V.
What solution will be available in hardware or software (in triggered mode)?
Thank's!
Hello Georgy,
While your system specifications are within the capabilities of the INA226 (low-side measurement, 5V<Vcm<30V), please ensure that the bandwidth is sufficient. The INA226's bandwith is only ~100Hz.
If you need a device that's a bit faster and has a built-in comparator, the INA200-208 family may be of interest. This is an analog-only solution, though. Also please be aware that the devices in that family require a sense voltage of >20mV for linear operation.
Hi, Pete!
Thank's You answer, It the INA226's bandwidth is only ~100Hz realised with the AVG bit settings 1024. If averages eq. 1 or 4 there be more fast processing. In other side with time I have wide range My abilities, there no problem.
INA226 is unique device with digital output, and other necessary data.