Other Parts Discussed in Thread: TLV4113
Hello Team,
I have a brief question regarding the TLV4113:
- When the pins are biased such that Vdd = 0V and shutdown = 0V, will the part be damaged if the negative input gets an approximately 1.5V and less than 2 mA signal? The part would only be in this condition for short periods of time.
Since the max ratings specify +/- Vdd on the input pins, I would think that over time this condition would damage the part, but I was hoping to receive some confirmation/clarification.
Thanks in advance,
Daniel Lanzone