This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Comparator LMV7219

Other Parts Discussed in Thread: LMV7219

Comparator needed as a zero-crossing detector.

In the beginning was the circuit 1. Comparator never switched.

Then I did the circuit 2. Comparator works, at the 3 input of the comparator is Um = 50mV. Watched broadband oscilloscope.

The generator should have the load 10 kohm±20%. Otherwise, not required frequency stability is guaranteed! The output signal (sine wave) is symmetric with respect to zero (the output is connected through a capacitor, which is inside the generator). The signal amplitude of generator is 0.5 V.

Question: How do I estimate the value of the generator load ? 

TIA

Vladimir Naumenkov  www.agat.by

1464.Circuit 1.pdf

2275.Circuit 2.pdf